{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I setup serial communication between a Twido and a Magelis HMISTU655 using TwidoSoft v3.5?

Goals and Symptoms

This resolution provides a solution for setting serial communication between a Magelis HMISTU655 and a Twido. The RS485 port 1 and port 2 will be used on the Twido to communicate to a HMISTU655 HMI.

 

Causes and Fixes


Hardware:
TWDLCDA24DRF : Twido Compact PLC
TWDNAC485D: RS 485 connection module for Compact base
HMISTU655: Magelis HMI 3.5"

XBTZ9780 cable: Serial communication cable:
(or XBTZ978 + XBTZN999 adapter)

Software:
Twidosoft v3.5
Vijeo Designer v5.1

 

1) Setup the Twido Port 1 with the following parameters:
Type: Modbus
Address: 1
Baudrate: 19200
Data Bits: 8 (RTU)
Parity: None
Stop Bits: 1
Response Timeout: 10
Inter-frame delay: 10

Comm

Note: Parity must be set to None on Port 1.

 

2) Configure the TWDNAC485 optional port.
port

 

3) Setup the Twido Port 2 TWDNAC485 with the following parameters:
Type: Modbus
Address: 1
Baudrate: 19200
Data Bits: 8 (RTU)
Parity: None
Stop Bits: 1
Response Timeout: 10
Inter-frame delay: 10

comms

Note: Parity can be set to None or Even on Port 2 using the TWDNAC485D.

 

4) Create the following Ladder section.

comms

This initialize the memory words so that the TWIDO can communication to the HMISTU655. In a real application this may not be required.

 

5) In Vijeo Designer, configure the Modbus RTU serial driver with the following parameters:

Serial Interface: RS485
Transmission Speed: 19200
Retry Count: 2
Parity Bit: None
Stop Bit: 1
Rcv. Time Out: 1 (Sec)
TX Wait Time: 10 (Msec)
config

 

6) In Vijeo Designer, configure the Modbus EQUIPMENT with the following parameters:

Slave EQUIPMENT Address: 1
Preferred Frame Length: Custom, 120 bytes
IEC61131: 0-based
Word Order: High Word First
ASCII Display: Low byte first
config

 

7) Create a Integer variable link to %MW10 in Vijeo Designer
variables

 

8) Add a Numeric Display field and configure as shown below:
settings

Attachments

(Removed File URL: 202708_F0BE/HMISTU655.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/441585c9b16dbd42c125774b0010cccf/fl_block_5/0.544?OpenElement&FieldElemFormat=gif)(Removed File URL: 202708_F0BE/Twido.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/441585c9b16dbd42c125774b0010cccf/fl_block_5/0.1116?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL202708 V1.0, Originally authored by MiMe on 06/23/2010, Last Edited by MiMe on 06/23/2010
Related ranges: Twido

Schneider Electric Nigeria

Attachment(s)
Twido.zip [2.38 KB]
HMISTU655.zip [8.47 KB]
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.