{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Solution of light indication for 400V to 600VAC application ?

Goals and Symptoms

Solution of light indication for 400V to 600VAC application ?

Facts and Changes

LED blocks
Pilot lights
400V
600V

Causes and Fixes

For 440V application, you can use transformer blocks for 24V LED blocks, that will be implemented being the first row of contacts and Led.
400V => ZBV5B
440V - 460V => ZBV8B
550V - 600V => ZBV9B


Legacy KB System (APS) Data: RESL203836 V1.0, Originally authored by LaBe on 12/30/2010, Last Edited by LaBe on 12/30/2010
Related ranges: Harmony XB4

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: