{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a first scan bit available in SoMachine or EcoStruxure Machine Expert?

Article available in these languages: Spanish

Issue
How do I logically determine the first Task Cycle in a SoMachine or EcoStruxure Machine Expert PLC?

Product Line
SoMachine (Versions: v2.0, v3.1, v4.0, v4.1, v4.2, v4.3)
- PLCs: M238, M258, HMISCU
EcoStruxure Machine Expert (Versions: v1.1, v1.2.x, v2.0, v2.1)
- PLCs: HMISCU, M241, M251, M262

Environment
PLC programming software for Windows PC -> Logic Builder -> POU program

Resolution
The functions "IsFirstMastColdCycle" and "IsFirstMastCycle", is True during the first MAST task cycle after a start.

For example, with this small program in Structured Text:
(a and b are INT variables)

IF IsFirstMastColdCycle() 
    THEN
        a := a + 1;
END_IF
IF IsFirstMastCycle()
    THEN
        b := b + 1;
END_IF


Result:
The value of "a" will be 1 the first time that the PLC starts (Cold Start).
The value of "b" will increments each time that the PLC stops and starts (Warm Start).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: