{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I set a T function on relay RE11RMXMU?

Goals and Symptoms

How can I set a T function on relay RE11RMXMU?
Customer wants to use bistable relay function which is marked as Tl function. On the product the switch to the position Tl/Tt and connect the Y1 contact in order to control this function but he claims that there is no possibility to set infinite value on time range.
According functional diagram for bistable relay function the time between two pulses is infinite. But the relay all the time starts to count the delay according the position of potentiometers (time range and time unit).
How is possible to get infinite time between two pulses generated by Y1 contact?

Facts and Changes

RE11RMXMU

Causes and Fixes

You have to select the range selector 10-100h and adjust the unit potentiometer at maximum => 10, then the time is infinite between two pulses on Y1.


Legacy KB System (APS) Data: RESL204210 V2.0, Originally authored by LaBe on 12/30/2010, Last Edited by LaBe on 02/15/2011
Related ranges: Zelio Time

Schneider Electric Nigeria