Goals and Symptoms
How to transfer a Vijeo designer project from a PC with the OS Win 7 (64 bits) to a target type Magelis XBTGT1000 serie using XBTZG925 cable?
Facts and Changes
When using Vijeo Designer V6.1 installed on a PC with the OS Windows 7 (64 bit) and a XBTGT1100 terminal : the problem is that we cannot install the XBTZG925 cable driver.
Causes and Fixes
This is a limitation. There is only a Win XP XBTZG925 cable driver.
The reason is that Marketing decided that the target type XBTGT1000 serie End Of Commercialization and End Of Service will be in end of 2012.
The solutions are:
1/ either edit the Vijeo designer project on a PC with Win XP Pro,
2/ either replace the XBTGT1000 serie by a terminal type XBTGT1005 serie,
3/ or replace the XBTGT1000 serie by a terminal type XBTGTO
Note that solutions 2/ & 3/ with new terminals are less expansive and higher quality.
Legacy KB System (APS) Data: RESL209008 V1.0, Originally authored by DaBr on 09/05/2012, Last Edited by DaBr on 09/05/2012
Related ranges: Magelis XBT GT
Released for:Schneider Electric Nigeria