{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for the Twido TWDDRA16RT 16-point Discrete Output Expansion Module?

Issue:
What is the replacement for the TWDDRA16RT?

Product line:
Twido, OTB, TWD, TM2

Cause:
Product obsolescence.

Resolution:
The replacement is the Twido TM2DRA16RT 16-point Discrete Output Expansion Module. The Twido is obsolete and has been replaced with the M221 and now the TM2DRA16RT modules are also obsolete and that is now replaces with the TM3DQ16R. This will not work with the Twido's or the OTB"s.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria