{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Implementing CIP Explicit Message to Modbus Object between a M340 NOC401 (client) and a 140NOC78000 (server)

Issue
When using the 140NOC78000 as a server, to get process data through the Modbus object, only Unconnected_ Send messaging will work. The attachment is an example on how to perform an Explicit messaging using the DATA_EXCH block from a M340 NOC401 client.


Product Line
Quantum
140NOC78000
M340
BMXNOC0401


Environment


Resolution
Using UCMM and connected messaging will only return diagnostic data when communicating to a 140NOC78000.

Refer to Attachment

Schneider Electric Nigeria

Attachment(s)
BMXNOC0401_CIP_Modbus_Object_Read.ppt [325.5 KB]