{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What cables are available to be used with the BMXAMI0800 or the BMXAMI0810 ?

Issue:
What are the cable part numbers available for the BMAMI08xx modules?

Product Line:
M340, M580, x80

Cause:
Need cable options for the BMXAMI0800 and 0810 I/O modules.

Resolution:
There are two types of cables, each available in two lengths.
One 28-way terminal block on one end and flying leads on the other end.
BMXFTW308S - 3 meter (flying leads)
BMXFTW508S - 5 meter (flying leads)

One 28-way terminal block on one end and one 25-way D-sub connector on the other end for sub-bases (ABE7CPA02/03/31/31E).
BMXFTA150 - 1.5 meter ( molded 25 pin D connector)
BMXFTA300 - 3 meter    ( molded 25 pin D connector)

Schneider Electric Nigeria