{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What cables are available to be used with the BMXDDI1602 or the BMXDDO1602 ?

There is one type of cable, available in three lengths.
One 20-way terminal block on one end and flying leads on the other end.
BMXFTW301 - 3 meter
BMXFTW501 - 5 meter
BMXFTW1001 - 10 meter



Related ranges: Modicon M340

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: