Issue
This document is to clarify the published temperature specifications for the Advantys STB I/O range.
Product Line
Advantys STB
Resolution
Various approvals and certificates relevant to the application of the STB Distributed I/O product range may appear as contradictory to the published environmental characteristics of the STB range. The attached document states "the STB User Manual must be considered the reference for all environmental operating characteristics, and specifically, those characteristics related to temperature."
Attachments
(Removed File URL: 212223_DB92/Resolu_technique_STB_Temp_review_DC2.docx)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/299b8eabdeb7ebb2c1257bba00529a4a/fl_block_5/0.11A?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL212223 V1.0, Originally authored by DaDz on 08/01/2013, Last Edited by DaDz on 08/01/2013
Related ranges: Modicon STB
Released for:Schneider Electric Nigeria