Search FAQs
What is the default IP Address and credentials of an EGX100 or EGX300?
Issue
A user would like to know the default IP address, subnet mask, gateway, and credential information for an EGX100 or EGX300
Product Line
EGX100, EGX300
Environment
Communications
Cause
Default communication parameters are needed to establish a connection to the EGX100
Resolution
The default communication parameters are:
Default IP address | 169.254.0.10 |
Default Subnet Mask | 255.255.0.0 |
Default Gateway | 0.0.0.0 |
Default Username | Administrator |
Default Password | Gateway |
Default Frame Format | Ethernet II |
Default Media Type | 10T/100Tx Auto |
Default Obtain IP Address Automatically | Disabled |
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: