{}

Our Brands

Impact-Company-Logo-English Black-01-177x54
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
How can we help you today?
How many devices can be daisy chained off of the PNIM RS-485 ports?

Product Line
PNIM

Environment
RS-485

Resolution
The maximum number of devices that can be daisy chained out of the PowerLogic Network Interface Module (PNIM) RS-485 port are 32, without using repeaters. The maximum length of the daisy chain is dependent on the baud rate of the devices. See table below.

Typical maximum RS-485 Drive Distance

Baud Rate150-9600192003840057600115200
Distance (feet)40003200300023001600
Distance (meters)1220975914701488

*Note: Based on 24 AWG twisted shielded pair, 0.026 Ohm/ft (0.085 Ohm/m), 13pF/ft(41pF/m) conductor to conductor, 22 Pf/ft (72pF/m) conductor to shield.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.