Search FAQs
Can I order a CVMT for a CM4000T separately?
Issue
The CM4000T is shipped with one CVMT (Current Voltage Module). Is the CVMT sold independently of the circuit monitor in the case that a replacement is needed?
Product Line
CM4000T
Environment
Product Availability
Resolution
Yes, the Current/Voltage Module can be ordered separately.
The CVMT supports high speed transient detection.
Note: Previously, there was another type of Current Voltage Module. However, now the CVM42 is obsolete along with the CM4250. The CVM42 supported an anti-aliasing filter and was compatible with the CM4000 and the CM4250.
The CM4000T is shipped with one CVMT (Current Voltage Module). Is the CVMT sold independently of the circuit monitor in the case that a replacement is needed?
Product Line
CM4000T
Environment
Product Availability
Resolution
Yes, the Current/Voltage Module can be ordered separately.
The CVMT supports high speed transient detection.
Note: Previously, there was another type of Current Voltage Module. However, now the CVM42 is obsolete along with the CM4250. The CVM42 supported an anti-aliasing filter and was compatible with the CM4000 and the CM4250.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: