{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the CT wake up percentage of the Enercept Meter?

Issue:
What is the minimum current that the Intercept Meter's CT's can accurately read.

Product:
Enercept Meters

Environment:
Current Measurement

Resolution:
The minimum amount of current the Enercept meter can accurately read is 10% of the max rated current of the CT that the Enercept Meter was purchased with. The CT's will pick up current below this rating, however accuracy will diminish the lower the current goes.

Schneider Electric Nigeria