{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to use a three phase 120V L-N through a potential transformer for control power to the CM4000 that is 69V L-N
Issue
User wants to use three phase 120V L-N through a potential transformer for control power to the CM4000 that is 69V L-N

Product Line
CM4000

Environment
Wiring

Resolution
Yes, the circuit monitor can be used with line-to-line rated PT's connected line to neutral, which results in a line-to-neutral voltage of 69.

Schneider Electric Nigeria