{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum pulse width or duration required on a IOX or IOC module to register an input status change on the CM4000 series meter?
Issue
Minimum pulse or duration required on a IOX or IOC module on a CM4000 series meter

Product Line
CM4000 series meter

Environment
Hardware Specifications

Resolution
The minimal pulse duration per input on the CM4000 IOX or IOC is 15ms when the control power to the meter is DC voltage. For AC voltage to the control power the minimal input pulse duration is 23ms.

Schneider Electric Nigeria