{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the control power requirements for the Enercept Network Adapter (ENA)?

Issue
What are the control power requirements for the ENA?

Product Line
Enercept Meter, ENA

Cause
User would like to know control power range for ENA

Environment
Installing ENA

Resolution
The control power requirements for the ENA (Enercept Network Adapter) are as follows: 9-30Vdc or 12-24Vac ; not including power factor, 1.5W max, 125mA max @12Vdc, 65mA max @24Vdc.

Schneider Electric Nigeria