Search FAQs
Bad Pulse Rate" error appears on a 1600 amp Energy Meter
Issue
Energy meter error "bad pulse rate" appears on the front display of a 1600 amp Energy Meter
Product Line
Energy Meter
EME3164
Environment
Pulse Output Selection Availability
Cause
The default pulse setting (0.1), is not valid on 1600 A Energy Meter
Resolution
Change the pulse rate switch setting from 0.1 (default) to a value such as 0.25, 0.5 or 1.0 kWh/Pulse to clear the error.
For more information on Energy Meter Pulse out, refer to article FA260559
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: