{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the length of the current transformer wire that ships with the Energy Meter?

Issue
The user requires the length of the current transformer wires that ship with the Energy Meter.

Product Line
Energy Meters basic (EMB) and Extended Range (EME)

Environment
Energy meter (EMB and EME)

Resolution
The length of the current transformer wires that are shipped with the Energy Meter is Six feet, 72 inches or 2 meters.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: