{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the required CT wake-up percentage for the Energy Meter?

Issue:
Customer wants to know what is the minimum required percentage required for excitation on the Energy Meter.

Product Line:
EMB1010, EMB1021, EMB1032, EMB2010, EMB2021, EMB2032, EMB2043, EMB2083, EMB3010, EMB3010, EMB3021, EMB3032, EMB3043, EMB3083, EMB3084, EMB3164

Environment:
CT excitation

Cause:
CT's require a minimum excitation percentage.

Resolution:

According to Veris, a minimum of 2% is required.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.