{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Internal Modbus register list for CM3000 and CM4000 Series Meters
Issue
Modbus list is needed

Product Line
CM3000 Series
CM4000 Series

Environment
Modbus Communications to CM3000 and CM4000 meters

Cause
Register list is needed to read registers when not using ION Setup or Power Monitoring Expert


Resolution
See the attached Register List.
External CM4000 Series Register List can be found HERE

Schneider Electric Nigeria

Attachment(s)
Internal_CM3_CM4_Register_List_15_020.xls [4.88 MB]