{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION7650/7550 - Is Parallel Redundancy Protocol possible on meters?

Goals and Symptoms:
We would like to set up Parallel Redundancy Protocol (PRP) with the fiber optic ports. The meters will be connected in two/redundant LAN network to allows data to overcome any single network failure without affecting the data transmission.
The PowerLogic ION7550/ION7650 meters as I have seen has only a single fiber optic port. Are you developing to attain PRP support or is it already implemented?
----------------------------------------------------------------
Facts and Changes:
fiber, fiber, optic, LAN, dual
----------------------------------------------------------------
Causes and Fixes:
The meters are not capable of it today. In hardware, you can get 1 ethernet port, 1 fiber port, or 1 ethernet and 1 fiber port. There is no option for 2 fiber ports and there is no option for 2 ethernet ports.
In firmware, the meter only accepts configuration data for 1 network.
It is possible that in the future we would expand the hardware options to offer 2 ethernet ports and expand the firmware to allow 2 networks to be configured but we are not likely to ever offer 2 fiber ports."


Legacy KB System (APS) Data: RESL206914 V1.0, Originally authored by MiGe on 12/22/2011, Last Edited by MiGe on 12/22/2011
Related ranges: ION7550/ION7650

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.