{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to change the parity of a direct serial site in ION Enterprise

ION Enterprise assumes that a device being added into the Management Console is set to 'NONE' for the parity. If the device is set to 'EVEN', the direct site configuration must be changed from 'NONE' to 'EVEN'. The parity settings are accessed through the Advanced Properties of the Site configuration:
1. In the Management Console, click on the Sites button to view the added sites.
2. Right-click on the serial site and select Configure Site.
3. Once the site is open, right-click in the empty grey space and select Advanced Properties.
4. Scroll toward the bottom to locate the Parity setting and then change the configuration as needed.

For a step-by-step process with screen shots, please view the attached documentation.

IONE_EVEN_parity.doc


Legacy KB System (APS) Data: RESL208155 V1.0, Originally authored by DaDu on 05/15/2012, Last Edited by DaDu on 05/15/2012
Related ranges: ION Enterprise V6.0

Schneider Electric Nigeria