{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION Enterprise Monthly Reset Peak Demand Power for PM800

Issue
There is no good way to reset Peak Demand on the PM800 series (or other Powerlogic Devices)

Product Line
ION Enterprise or SPM7, PM800

Environment
VIP

Resolution
The attached process will reset the Power Min/Max Demand at the start of every month, based on when the 'Clock' determines that a new month has began--not '30 days elapsed'.

This process can be used for other values that should be reset at the start of every month as well, so long as it is a value that the register is accessible via ION Enterprise.

Please check the attachments to download instruction file: 'Clock-Based_Reset_Instructions'.

Schneider Electric Nigeria

Attachment(s)
Clock-Based_Reset_Instructions.docx [229.34 KB]