{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

ION7300 Series Obsolescence (obsolete) End of Commercialization

Article available in these languages: Spanish

Issue
ION 73xx series Obsolescence (obsolete) End of Commercialization

Product Line
ION7300
ION7330
ION7350

Cause
Customer wants to order the ION73xx series meter but is it available for sale?

Environment
End of commercialization and recommended replacement

Resolution
The end of commercialization date is January 31, 2016, with a last time buy date is January 8, 2016, subject to product availability.

NOTE: The direct replacement for the ION 7330 and ION 7350 meters is the PM8000 series meter (Part Number: METSEPM8240).

The ION73xx will continue to be repaired until December 2017 as parts allow.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: