{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How can you modify the number of backups retained in PME?

Issue
A user may want to modify the number of backups retained in PME

Product Line
Power Monitoring Expert 7.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Windows Task Manager

Cause
In PME 7.2 and greater, scheduled tasks have been removed from the ION Database Manager and are now handled by the Windows Task Scheduler which invokes Windows PowerShell files to run the backup. The PowerShell file itself will need to be modified to change the number of backups.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).*

Navigate to the following directory < >\Power Monitoring Expert\config\cfg\DbScheduledTasks (may vary depending on the installation directory) and open the file "Backup.ps1" either with Windows PowerShell or Notepad and edit the code as shown below.
Original Code:

powerschell script

Modified Code:

powershell script

Save the file to retain the changes.

The following video demonstrates how to perform this configuration.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: