{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do the program and data get stored in the memory of Quantum PLC

In case no memory extension card is used with PLC, then the program data and constants are stored in the internal RAM memory of the processor module only.
However, when the memory extension card is used with PLC, then data is stored in the internal RAM memory of processor module, whereas programs and constants are stored in the memory extension card.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: