{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Unable to select device in Modbus Import Module when connecting to an external Modbus master and downstream slave using VIP

Issue
In the VIP, the Modbus Import Modules properties shows "Not_a_valid_device" when trying to select the Device Name.
Module setup Modify Enumerated Register

Product Line
ION meters

Environment
ION Enterprise 5.5

Struxureware Power Monitoring 7.0(SPM)

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x


Cause
'MI1 Device Name' shows, "Not_a_valid_device" because no modification of the Virtual Processor Setup tool was done.

Resolution
The ION Virtual Processor Setup must be configured to include the desired Modbus network. The following procedure explains how to add the Modbus network in the ION Virtual Processor Setup:

  • Access the ION Virtual Processor Setup via Management Console > Tools.
  • Expand the Modbus Network item.
  • Add a new Master site.
  • Expand the Master site and add a Device

See attachment for more information.

Schneider Electric Nigeria

Attachment(s)
VIP_connecting_to_an_external_modbus_master_and_downstream_slave.pdf [151.08 KB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: