{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why does the Series 3000/4000 Circuit Monitor display show stars or asterisks for frequency?

Issue
Why does the Series 3000/4000 Circuit Monitor display show stars or asterisks for frequency?

Product Line
CM3000 and CM4000 series meter

Cause
Customer see stars or asterisks for frequency on CM3000 or CM4000 front display.

Environment
Reading Frequency from front display on CM3000 or CM4000 meter.

Resolution
There are several possibilities in which this could occur:

  1. The frequency is changing too quickly. (Possible causes could be when monitoring a Generator that has not stabilized the voltage frequency)
  2. The voltage on phase A and C has dropped to zero. (Normal)
  3. (CM4000 series only) The Current Voltage Module (CVM) module is not properly seated. (NOTE: In this instance cycling control power to the meter will not help.)
  4. (CM4250 Only) This symptom can also be caused by the temperature chip in the meter when the firmware version is earlier than 14.4. To confirm this is the issue read register 3238. If the value is zero, then this may not be the issue. It is recommend that the firmware be upgraded to the latest version available.
  5. If none of these solutions work then use the attached flow chart to validate the issue and contact the appropriate group per the PDF attachment.

Schneider Electric Nigeria

Attachment(s)
PMC-Corrective_Action_Plan_PMC-HW-CM4-0002.pdf [29.9 KB]