{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the EM4800 wired for Delta Service Configuration using PTs

Issue:
Customer is looking to wire EM4800 as Delta configuration.

Product Line:
EM4800

Environment:
EM4800

Cause:
Diagram needed for delta configuration

Resolution:
The attached document provides the wiring diagram for an EM4800 metering Delta Service using PTs (600V: 120 V).
Delta Service Configuration.vsd


Schneider Electric Nigeria