{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the recommended CT part numbers for the EM3500 meters?

Issue
What are the recommended CT (current transducer) part numbers for the EM3500 meters?

Product line
EM3500 series meter

Environment
Current connection with EM3500 series meter

Resolution
Low-Voltage (0-1/3 V) Split Core current transducer part numbers are available as shown in table below:


Part Number Description
Image 1

NOTE: These CTs will only work with the EM35xx series; they will not work with EM35xxA. For CTs that will work with the EM35xxA refer to FA233732. The EM35xx will accept either 1/3 V or 1V secondaries.

Size details shown in table below. Image 2

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: