{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
WebReach Generates Many Event Viewer Events if Devices are Slow to Respond

Goals and Symptoms


Summary

WebReach can generate many events in the OS Application Log if devices are slow to respond. This article describes how to add a Registry value to increase the allowable response time.


Symptoms

A glance at the Event Viewer Application Log reveals a steady stream of errors logged by VBRuntime. For example:

-----------------------

The VB Application identified by the event source logged this Application PMLWebReachReadMeter: Thread ID: 2692 ,Logged: WebReachReadMeter Failing x-pml:/Diagrams/ud/Default/3720_FAC-4WYE_V1.1.0/3720_FAC-4WYE_V1.1.0.dgm@direct.3720_73 because no response received by 27/06/2005 10:18:57 AM. Request initiated at 27/06/2005 10:18:24 AM. Elapsed time 33.000000170432 limit is 31

----------------------

Facts and Changes

Keywords

WebReach

WebReachReadMeter

Event Viewer

VBRuntime


More Information

This event was added to provide some additional trouble-shooting diagnostics for WebReach in ION Enterprise 5.0 Service Pack 4.

Causes and Fixes

Cause

The default response time limit for WebReach is set to 31 seconds. If a response fails to return within this limit, an event is written to the Event Viewer Application Log.
Resolution

If a system includes devices that are consistently very slow to respond for some reason, you can add the following registry value to increase the response timeout value.

Add a DWORD value called FailAfterNoResponse to the WebReach registry key and set it to an appropriate value so that the Event Viewer will not fill with unnecessary events.

Alternatively, reconfigure the system so that the devices are not so slow to respond.

Original article#11710


Legacy KB System (APS) Data: RESL182932 V1.0, Originally authored by DaMi on 03/20/2007, Last Edited by DaMi on 03/20/2007
Related ranges: ION Enterprise

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.