{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Launching Module Will Not Operate When Using Source Inputs

Goals and Symptoms


Summary

When referencing the Source inputs of a Launching module, incorrect syntax in the RunCommand setup register will prevent the Launching module from executing correctly.

Symptoms

The Launching module does not execute correctly. For example, when the Launching module is pulsed and its Launch Mode setup register is set to Interactive, a command prompt window flashes briefly on screen then disappears.  However, when the reference to the Source inputs is removed from the RunCommand setup register, the Launching module operates correctly.

Facts and Changes

Keywords

Launching module, ION Enterprise

More Information

See KB article#9505 and article#9851.

Causes and Fixes

Cause

Spaces are not permitted in the syntax of the RunCommand setup register when that RunCommand setup register references the Source inputs.

Resolution

Ensure that there are no spaces within the RunCommand setup register path when the Source inputs are referenced within the Launching module.

Original Article#11642 (preceded by article#11641)


Legacy KB System (APS) Data: RESL182943 V1.0, Originally authored by DaMi on 03/20/2007, Last Edited by DaMi on 03/20/2007
Related ranges: ION Enterprise

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.