Search FAQs
Does the Imax on the Bar Graph Display show half cycles on the ION7650/7550?
Product Line
ION7650/7550
Environment
Measurements
Resolution
The Max Current used in the front panel display is based on a 1sec update RMS calculation, so its going to be the 1sec Max current value since the last Max reset occurred.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: