Search FAQs
What is the maximum KYZ cable length that can be used for an 8600 meter?
It is difficult to say because it depends on many variables such as the cable type (characteristic impedance), the voltage, the length (duration) of the pulse and the sensitivity of the receiver input.
Last Revised: 3 October 2007
Public
All content © 1992-2007 Schneider Electric
Legacy KB System (APS) Data: RESL188302 V1.0, Originally authored by KBAdPM on 10/04/2007, Last Edited by KBAdPM on 10/04/2007
Related ranges: ION8600
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: