{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to perform an IIS Reset using Command Prompt.

Article available in these languages: Czech

Issue
iisrest can help with many web-based bugs, errors, or issues in the power monitoring expert software

Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 9.1
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Windows
Command Prompt
Intranet Information Services
PME Web Applications

Resolution

  1. Open the Command Prompt. Click on Start > All Programs > Accessories > Command Prompt
Note: It may be necessary to right-click on the Command Prompt icon and select "Run as Administrator" if the following steps fail with a warning stating the task requires elevation.
  1. Once the Command Prompt window opens, type 'iisreset' (without quotes) and then press Enter
iisreset
  1. Once the message "Internet services successfully restarted" is displayed, close out of the Command Prompt
iis complete

Schneider Electric Nigeria