Issue
DNP3.0 requires a unit ID even if it is over ethernet.
Product Line
ION 7500, ION7600
Environment
IONSetup
Cause
The framework in an ION7600 does not allow you to set the DLAddress for ethernet (which is essentially the unit ID).
Resolution
NOTE: all devices and COM ports must have unique device IDs, and all operate at the same baud rate.
- Set COM2 to Ethergate
- Connect the twisted shielded pair (RS485) between COM1 and COM2
- Set the protocol on COM1 to DNP3.0 then set the unit ID to the desired number.
Released for:Schneider Electric Nigeria
Issue
DNP3.0 requires a unit ID even if it is over ethernet.
Product Line
ION 7500, ION7600
Environment
IONSetup
Cause
The framework in an ION7600 does not allow you to set the DLAddress for ethernet (which is essentially the unit ID).
Resolution
NOTE: all devices and COM ports must have unique device IDs, and all operate at the same baud rate.
- Set COM2 to Ethergate
- Connect the twisted shielded pair (RS485) between COM1 and COM2
- Set the protocol on COM1 to DNP3.0 then set the unit ID to the desired number.
Released for:Schneider Electric Nigeria