{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a ION7300 meter with the Profibus option use other protocols?

Issue
User needs to know if an ION7300 with the Profibus option can use other protocols in addition to Profibus

Product Line
ION7300

Environment
Protocols

Resolution
Yes, the ION7300 meter with the Profibus option is also equipped with RS-485 port COM1. COM1 can be used to communicate using Modbus RTU or the ION protocol.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.