{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Communication Port configuration on an ION 8600A meter with the C1 Comms option?

On an ION 8600A with the C1 communication option, the ports will be configured as:
Com1: RS 232/485 (selectable)
Com2: Modem
Com3: IR
Com4: RS 485
Network: Ethernet

Please note that, if the meter is RMICAN sealed, then the COM4 is going to be blank.




Last Revised: November 13, 2007
Applies To: ION 8600
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189171 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: ION8600

Schneider Electric Nigeria