{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a single meter monitor both sides of an isolated transformer and retain isolation?

Product Line
PowerLogic Meters
ION Meters

Environment
Monitoring

Resolution
No, a single meter can only monitor a single point. Accurate measurements require Vref, so isolation would be lost if both sides of the transformer were connected to it.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: