{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the settings for a serial powered optical probe?

For serially connected optical probes (which do not have PS2 pigtail power)like the UNICOM III. The correct settings would be:
In ION setup> >Serial> Settings the RTS or DTS needs to be set to "Force ON".


Legacy KB System (APS) Data: RESL189270 V1.0, Originally authored by KBAdPM on 11/17/2007, Last Edited by KBAdPM on 11/17/2007
Related ranges: ION Setup 2.1

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.