{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will ION Enterprise retain Historical data if a Meter node is deleted, then added again later with the same name?

As long as the node names remain the same, the historical data will remain intact since ION_Network and ION_Data reference logged data to the node names. If a device/node is deleted from Management Console, and a new device with the same name is created, that new device will map to the existing data in ION_Data.

Last Revised: November 22, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189570 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.