{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

ION 8500v280 downgrade fails

If an ION8500 has firmware version v280, it means that it is a RevB meter. This meter has be repaired with parts an ION 8600, which is why it has the unique "RevB" firmware.
All attempts to downgrade this meter to versions lower than v280 (using ION Enterprise or ION Setup) will fail.

Last Revised: November 23, 2007
Applies To: ION 8500
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189623 V1.0, Originally authored by KBAdPM on 11/24/2007, Last Edited by KBAdPM on 11/24/2007
Related ranges: ION Setup 2.0, ION Setup 2.1, ION8500

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: