Search FAQs
What is the accuracy of the phase angle measurement on the ION 7650?
The Power Harmonics Module has phase angle accuracy within (±0.5º x harmonic number); hence, the deviation may increase with higher harmonics. In addition, the Power Harmonics Module is limited to a 2 second update rate since the module is driven from the FFT modules, which have a 2 second update time.
Last Revised: December 3, 2007
Applies To: ION 7650
Public
All content © 1992-2007 Schneider Electric
Legacy KB System (APS) Data: RESL189894 V1.0, Originally authored by KBAdPM on 12/03/2007, Last Edited by KBAdPM on 12/03/2007
Related ranges: ION7550/ION7650
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: