{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to log VIP Events

The 'event priority' of the VIP Event Log is set to 192 by default. Most control actions need this to be adjusted to a more useful level. For example the AND/OR Module requires an event priorty of 15 on transition actions. To record these changes in the event log follow this procedure:

  1. Load ION Designer and open the VIP
  2. Open the AND/OR Module setup registers
  3. Change the AN# EvLog Mode to Log-On
  4. Open the EventLogCtl 1 setup registers in the VIP
  5. Change the EL1 Cutoff to your desired Event priorty level (15 for this example)
  6. Choose File -> Send & Save then close Designer
  7. Open the Microsoft Services and restart the ION LogInserter Service.

This should allow the VIP events to show up in a Event Log Viewer object, or the Global Event Log viewer (with the appropriate viewing priority filter).



Last Revised: April 17, 2008
Applies To: ION Enterprise 5.0 / 5.5 / 5.6
Original Author: LS
Public
All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191707 V1.0, Originally authored by KBAdPM on 04/18/2008, Last Edited by KBAdPM on 04/18/2008
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.