{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Series 200 and 700 Power Meter (PM200, PM700, PM750) Register List with 3.050 firmware functionality.
Issue
Modbus register for PM200 and PM700 is needed.

Product Line
PM200 and PM700 series

Cause
Modbus register map is needed for PM200 and PM700 series meters.

Environment
Reading Modbus register for PM200 and PM700 series meters.

Resolution
Review the attached Excel documents for a detailed modbus register list for PM200 and PM700 series meters.
The following link has modbus registers for all ION Meters: index?page=content&id=FA300088

Schneider Electric Nigeria

Attachment(s)
Series_PM200_PM700_Register_List.xls [149.5 KB]