{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cannot add a new ION Enterprise user in the user manager of the Management Console.

Verify that the Windows user or the Windows group that the Windows user is in has full control of the ION Enterprise folder. To do this do the following:
1) Navigate to the ION Enterprise folder on the server.
2) Right click on ION Enterprise and go to properties.
3) Click on the Security tab.
4) Verify that the user or group in use has full control as shown below in the screenshot.



Date Created: February 25, 2009
Last Revised: April 29, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198393 V1.0, Originally authored by MiNe on 04/30/2009, Last Edited by MiNe on 04/30/2009
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.