{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to change the scale of the axis on the scrolling graph display of a numeric object in the Vista application

Issue
A user wants to change the scale of the axis on the scrolling graph display of a numeric object in the ION Enterprise/Power Monitoring Expert Vista application.

Product Line
ION Enterprise 6.0,
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Environment
Diagram modifications in the Vista application.

Resolution
Follow the steps below in order to change the scale on the scrolling graph display from Vista. There is also a step-by-step video embedded in this article which provides guidance on how to change the scale of the axis on the scrolling graph display in Vista.

1) Right click on the scrolling graph display with the toolbox open in Vista.
2) Go to the display tab and you will see a preview screen of your graph shown by the red box below.


3) Right click on the axis that you want to scale shown by the red and blue boxes below


4) By right clicking the axis it will bring up the axis properties that you can edit as shown above.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.