{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Maximum Real Energy (kWh) Accumulation Value Possible on an Enercept or Energy Meter?

Although, the real energy consumption is stored as a 32-bit floating point value and is held across two registers, the max kWh value is not equal to 4,294,967,296 kWh (which is 2^32). Instead, the maximum real energy accumulation is dependent upon the model of enercept or energy meter. See the table below.
CT Size kWh/Count Max 32-bit Accumulator Max kWh
100 0.0078 4,294,967,296 33,554,432
200 0.15625 4,294,967,296 67,108,864
300/400 0.03125 4,294,967,296 134,217,728
800 0.0625 4,294,967,296 268,435,456
1600 0.125 4,294,967,296 536,870,912
2400 0.25 4,294,967,296 1,073,741,824


Legacy KB System (APS) Data: RESL199011 V1.0, Originally authored by AnVa on 05/28/2009, Last Edited by AnVa on 05/28/2009
Related ranges: PowerLogic Energy Meter, Enercept

Schneider Electric Nigeria