{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can Microsoft Outlook Express be used with ION Enterprise Reporter instead of Microsoft Outlook?

Yes, it is possible to use Microsoft Outlook Express instead of Microsoft Outlook to send out an email with ION Enterprise Reporter. Microsoft Outlook Express must be installed on the same machine as ION Enterprise Reporter to work properly.

Date Created: November 24, 2009
Last Revised: November 25, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200599 V1.0, Originally authored by MiNe on 11/26/2009, Last Edited by MiNe on 11/26/2009
Related ranges: ION Enterprise V6.0, ION Enterprise V5.6, ION Enterprise V5.5

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.